AXIS#.BODE.INJECTPOINT

Description

AXIS#.BODE.INJECTPOINT sets whether the excitation uses current or velocity excitation type.

AXUS#.BODE.INJECTPOINT Description
0 None
1 Current
2 Velocity

Example

Set AXIS1.BODE.INJECTPOINT to current:

--> AXIS1.BODE.INJECTPOINT 1

Get AXIS1.BODE.INJECTPOINT (already set to current):

--> AXIS1.BODE.INJECTPOINT 1

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 2
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
AXIS1.BODE.INJECTPOINT

5001h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.BODE.INJECTPOINT

5101h

01h

Unsigned8

-

-

Read/Write

No